Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Ground Straps

We can't find products matching the selection.

Industrial Grounding Straps for Bonding, Static Control, and Equipment Safety

Industrial grounding straps (also commonly called bonding straps) are used to create a low-resistance connection between conductive components so electrical faults and static charges have a safe path to ground. In manufacturing and maintenance environments, they're most often used to bond enclosures, control panels, doors, motors, cable trays, and movable machine elements that might otherwise develop a voltage potential. When you're selecting grounding straps for industrial use, it helps to start with the broader connectors, cordsets & terminals ecosystem and then narrow to the correct grounding solution for your application.

For correct selection, prioritize the factors that impact electrical performance and long-term reliability: required current capacity (including fault current), strap length (keep it as short as practical), conductor construction (braided vs. laminated), and connection method (stud-hole, lugged ends, or hardware kits). Braided grounding straps are common where flexibility and vibration resistance matter-such as bonding a panel door to the enclosure-while wider straps can be helpful when you need lower impedance at higher frequencies (relevant for noise and EMI considerations). If your strap will live near heat, oils, washdown areas, or corrosive environments, pay close attention to plating/material compatibility and consider whether the broader grounding approach should include additional components within grounding to support consistent bonding practices across equipment.

Proper usage matters as much as the strap itself. A grounding strap can only do its job if it's installed on clean, conductive surfaces with secure hardware and protected from loosening over time. For example, paint, powder coat, oxidation, and contamination can all increase resistance at the connection point, undermining the bond even if the strap is correctly sized. In industrial control and automation builds, grounding and bonding practices are often part of a larger electrical safety strategy that may also involve routing, shielding, and component selection in automation and control panels.

Frequently Asked Questions

What's the difference between grounding and bonding straps?

In industrial contexts, a "grounding strap" is often used to describe a strap that connects metal parts to a grounding system, while "bonding" emphasizes equalizing potential between conductive parts (like an enclosure body and its door). In practice, many straps serve both purposes: they provide a low-resistance path that helps minimize shock hazards, reduce nuisance issues caused by static discharge, and support predictable equipment operation. If you're comparing options for different assemblies, start in the grounding category and choose straps based on how the equipment moves, vibrates, or needs to be serviced.

How do I choose the right size and length for an industrial grounding strap?

Choose a strap sized for the electrical demands of the application (including fault conditions where applicable), then select the shortest length that still allows for movement without putting stress on the terminations. Overly long straps can add resistance/impedance and create awkward routing that gets snagged during maintenance. If the strap is being used on a moving door, hinge, or vibration-prone assembly, prioritize flexibility and strain relief. For applications where grounding is part of a broader wiring/termination plan, it can also help to review related connection options within connectors, cordsets & terminals.

Where are grounding straps commonly used in industrial facilities?

Grounding straps are frequently used to bond enclosure doors to the main enclosure body, bond equipment frames and panels to a grounding point, and provide continuity across hinged or removable sections where a hard conductor would fatigue or break. They can also be used in static-sensitive areas to reduce electrostatic discharge risk when paired with a properly designed grounding approach. If your facility includes sensitive controls, drives, or instrumentation, grounding and bonding decisions may tie into your overall reliability strategy across automation and control and process instrumentation systems.