Resolvers

We can't find products matching the selection.

Resolvers for Motor Feedback and Precision Motion Control Systems

Resolvers are electromechanical feedback devices used to measure the angular position, speed, and direction of rotating shafts in industrial motion control systems. These sensors convert mechanical motion into electrical signals that can be interpreted by controllers and motor drives, enabling accurate monitoring and regulation of motor performance in automated equipment.

In industrial automation, resolvers are commonly used in servo motor and drive applications where precise feedback is required to maintain consistent motion profiles and positioning accuracy. By providing continuous analog signals that represent shaft angle and rotational velocity, resolvers help control systems adjust motor input to match process demands and maintain stable operation.

A resolver typically consists of a stationary stator and a rotating rotor arranged in a transformer-like configuration. When energized with alternating current, electromagnetic coupling between the windings produces sine and cosine output signals that correspond to shaft position. These signals are processed by control electronics to determine the exact angular displacement of the motor shaft.

Resolvers are valued in industrial environments for their rugged construction and ability to operate reliably under harsh conditions such as high temperatures, vibration, dust, moisture, and mechanical shock. Because they contain minimal onboard electronics and rely on simple electromagnetic principles, resolvers often provide longer service life and improved reliability compared to some other feedback technologies in demanding applications.

Common applications for resolvers include robotics, CNC machinery, conveyors, packaging equipment, elevators, and other automated production systems that require accurate closed-loop motor control. Proper resolver selection depends on factors such as resolution requirements, mounting configuration, electrical interface compatibility, environmental exposure, and integration with servo drives or motion controllers.

By enabling precise motor feedback and supporting advanced motion control strategies, resolvers play a critical role in improving automation performance, reducing mechanical wear, and maintaining consistent process efficiency in industrial drive systems.

Frequently Asked Questions

What is resolver resolution?

Resolution refers to how accurately the system can determine shaft position based on the resolver's output signal processing.

Do resolvers require calibration?

Initial system setup may require calibration or alignment to ensure accurate position feedback and optimal control performance.

What mounting methods are used for resolvers?

Resolvers may be directly mounted to motor shafts or connected using couplings or hollow-shaft configurations.