Galco will be closed Friday, July 3, for Independence Day.

Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Grips

We can't find products matching the selection.

Cable Grips for Pulling, Support, and Strain Relief

Cable grips are used to hold, support, and guide cable in industrial electrical installations where pulling force, mechanical strain, or long suspended runs could damage the cable or its termination point. Their woven mesh construction grips the cable jacket along a broader section of the cable, helping distribute load more evenly than a single attachment point. In industrial environments, cable grips are commonly used during cable installation, for ongoing support, or to reduce strain at equipment and enclosure entry points.

Different cable grip types are designed for different functions. Pulling grips are often used to help guide cable through conduit, tray, or other routing paths during installation. Strain relief grips help reduce tension at cable entry points and terminations, while support grips are used to help carry cable weight in vertical or suspended applications. Choosing the right grip helps protect the cable, improve handling, and support longer service life in demanding industrial settings.

Galco offers cable grips for a wide range of power and wiring applications. The correct selection depends on cable diameter, load requirements, installation method, and whether the grip will be used for pulling, support, or strain relief. Proper grip selection helps improve cable handling, reduce mechanical stress, and support more reliable installations across power and electrical systems.

How to Choose the Right Cable Grip

Selection starts with how the grip will be used. Some applications involve temporary pulling during installation, while others require long-term support or ongoing strain relief at a cable connection point. Matching the grip type to its intended function is just as important as matching it to the cable itself. Cable diameter range, cable weight, mesh style, and attachment method all affect whether the grip will perform correctly in the application.

Installation conditions also matter. Vertical runs, suspended cable, vibration, and repeated movement can place added stress on both the cable and the grip, which may call for a heavier-duty or more specialized design. In some systems, cable grips are used alongside related cable management and entry components such as cable entries and wireholders to support a more secure and organized installation.

Frequently Asked Questions

What is a cable grip used for?

A cable grip is used to hold and support the cable during installation or in permanent service. Depending on the design, it can help pull cable through a routing path, reduce strain at a termination point, or support the weight of cable in suspended or vertical applications.

How do I choose the right cable grip?

Start by identifying whether the grip will be used for pulling, strain relief, or long-term support. Then match the grip to the cable diameter, load requirements, and installation method. It is also important to consider whether the application involves vertical load, vibration, or frequent movement.

What is the difference between pulling grips, strain relief grips, and support grips?

Pulling grips are used to help guide cable during installation, strain relief grips help reduce mechanical tension at cable entry or connection points, and support grips are used to help carry the weight of cable in hanging or vertical applications. The right choice depends on how the cable needs to be handled and protected.