Power Centers

We can't find products matching the selection.

Power Centers for Portable Industrial Power Distribution

Power centers are used to distribute incoming electrical power to multiple receptacles from a single unit, helping support temporary equipment setups, maintenance work, jobsite power access, and localized industrial operations. In many applications, they provide a safer and more organized way to bring power closer to the point of use without relying on multiple separate extension or connection points.

Industrial power centers are often selected based on how power enters the unit, what receptacles are available at the output, and what built-in protection features are required for the environment. Depending on the design, a unit may include duplex receptacles, locking outlets, power feed-through capability, GFCI protection, overload protection, and enclosure features intended to support more demanding work conditions. These details can make a significant difference in whether a power center is suitable for the equipment and environment it will serve.

Galco offers power centers for industrial electrical applications where portable or localized power distribution is needed. Choosing the correct power center depends on input and output voltage, current rating, receptacle configuration, inlet type, protection features, and the environmental conditions of the application. Proper selection helps support safer power access, improve equipment usability, and maintain a more organized electrical setup across power and electrical systems.

Choosing the Right Power Center for the Application

Selection starts with the incoming power source and the types of equipment that need to be connected. Input voltage, output voltage, current rating, and inlet type all need to match the available power and the demands of the tools or equipment being served. Receptacle layout is also important, especially when a single unit needs to support multiple connection types such as duplex outlets, locking receptacles, or higher-amperage power connections.

Built-in protection and environmental suitability should also be considered before choosing a unit. Features such as GFCI protection, overload protection, flip covers, and power feed-through capability can affect both safety and usability, depending on where and how the power center will be used. In some applications, NEMA rating and receptacle protection are especially important where moisture, dust, traffic, or rough handling are part of the operating environment. Power centers are often used alongside related distribution products such as plugs and receptacles and safety switches depending on how power is delivered and managed across the site.

Frequently Asked Questions

How do I choose the right power center?

Start by matching the available input power to the unit's input voltage, inlet type, and current rating. Then confirm that the output receptacles and voltage match the tools or equipment that need to be powered. Protection features and environmental rating should also be considered based on where the unit will be used.

What power center features matter most for industrial use?

Important features often include receptacle configuration, current capacity, GFCI protection, overload protection, flip covers, and whether the unit includes power feed-through capability. The right combination depends on the type of equipment being powered and the conditions of the work environment.

When do I need a power center with GFCI protection or power feed-through?

GFCI protection is often important in applications where personnel protection and wet or demanding environments are a concern. Power feed-through can be useful when the unit needs to support downstream distribution or allow additional equipment to be powered from the same source. The right choice depends on how the unit will be used in the field.