Galco will be closed Friday, July 3, for Independence Day.

Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Power Strips

We can't find products matching the selection.

Power Strips and Service Poles for Localized Power Distribution

Power strips and service poles are used to distribute electrical power to multiple devices from a single source, helping support workstations, equipment areas, and temporary setups in industrial and commercial environments. Power strips typically provide multiple outlets in a compact format, while service poles are designed to bring power down from overhead systems to desks, benches, or floor-level equipment. Together, they help make power more accessible where it is needed without requiring permanent rewiring.

Different configurations are designed to support different use cases. Standard power strips are commonly used to expand outlet availability at a fixed location, while service poles are used where power needs to be routed from ceilings to work areas in a more structured and permanent way. The right solution depends on how power needs to be delivered, how frequently connections change, and how the workspace is organized.

Galco offers power strips and service poles for a range of industrial and commercial power distribution applications. Choosing the correct product depends on input voltage, output capacity, number of outlets, protection features, and how the unit will be installed and used. Proper selection helps support safer power access, reduce clutter, and improve usability across power and electrical systems.

How to Choose the Right Power Strip or Service Pole

Selection starts with the electrical requirements of the application. Nominal input voltage, frequency, and total output capacity must align with the equipment being powered. The number and type of outlets should match the devices in use, especially when multiple pieces of equipment need to be connected at the same time. Built-in circuit breakers can also be important for protecting connected devices and preventing overload conditions during operation.

Additional features and installation conditions should also be considered. Some applications benefit from added protection, such as network or telephone surge protection, while others prioritize physical layout and accessibility. Service poles are often used where power needs to be routed from overhead to workstations in a clean and organized way, while power strips are better suited for expanding outlet access at a fixed location. In some systems, these products are used alongside related components such as power centers and plugs and receptacles depending on how power is distributed throughout the facility.

Frequently Asked Questions

What is the difference between a power strip and a service pole?

A power strip provides multiple outlets from a single connection point and is typically used at a fixed location. A service pole is used to route power from an overhead source down to a workstation or equipment area, helping organize power delivery in spaces where floor or wall outlets are not easily accessible.

How do I choose the right power strip?

Start by matching the input voltage, output capacity, and number of outlets to the devices being powered. Then consider whether features like circuit breakers or additional protection for communication lines are needed based on the application.

When should I use a service pole instead of a power strip?

A service pole is typically used when power needs to be delivered from an overhead source to a workstation or open floor area. It is a better fit for more permanent or structured layouts, while power strips are often used to expand outlet access at existing connection points.