Rocker Switches

We can't find products matching the selection.

Industrial Rocker Switches for Panel and Equipment Control

Rocker switches are maintained-contact operator interface devices that control one or more circuits through a pivoting actuator, giving a clear visual indication of switch state at a glance. Within Galco's switches category they sit alongside toggle switches and pushbuttons as common operator interface choices, but their flat, panel-flush profile and large actuation surface make them particularly suited to applications where gloved operation, accidental actuation prevention, or a compact panel footprint are priorities. Unlike pushbuttons, which typically default to momentary action, rocker switches are most commonly specified in maintained configurations; the switch stays in its last position without continuous operator force.

Circuit configuration is the first selection parameter. SPST (single pole, single throw) handles straightforward on/off control of a single circuit and is the correct choice when nothing more than making or breaking one current path is needed. SPDT (single pole, double throw) routes a single input to one of two outputs, useful for manual/auto mode selection, speed selection, or switching a device between two operating states. DPST (double pole, single throw) switches two independent circuits simultaneously with one actuator, the standard choice for 240V AC loads where both line conductors must be interrupted together for proper isolation. DPDT (double pole, double throw) provides the most flexibility, functioning as two SPDT circuits in a single body, common in motor direction reversal and applications requiring simultaneous switching of two independent signal or power paths. Specifying a single-pole switch where a double-pole is required doesn't just create a control problem; in mains-voltage applications, it creates a safety hazard by leaving one conductor live when the switch reads "off."

Beyond configuration, current and voltage rating must match the actual load; pilot duty ratings for switching inductive control circuit loads, such as relay and contactor coils, differ from resistive load ratings and are not interchangeable. Illuminated rocker switches integrate an LED indicator into the actuator body to confirm circuit state, particularly useful in control panels where the switched load isn't directly visible from the operator position; LED indicators are preferred over neon for DC and low-voltage control circuits. For environments with coolant splash, solvent cleaning, or metal dust, IP65-rated sealed rockers prevent ingress that would degrade contact reliability over time. Where panel labeling is required, and in machine control it typically is, legend plates and switch accessories provide marking and protective options. For applications where variable output rather than discrete on/off control is needed, dimmer switches or selector switches are worth reviewing as alternatives depending on the control requirement.

Frequently Asked Questions

When should I use a rocker switch instead of a toggle switch?

Rocker switches and toggle switches are functionally equivalent in most circuit configurations - the distinction is mechanical and ergonomic. Rocker switches present a larger, flat actuation surface that sits flush or near-flush with the panel, making them easier to operate with gloves and less prone to accidental actuation from incidental contact. Toggle switches provide a more pronounced lever that offers clearer tactile feedback and tends to be easier to identify by touch alone in low-visibility environments. Panel space and operator interface requirements usually drive the choice more than electrical performance.

Do I need a DPST or DPDT rocker switch for a 240V AC application?

DPST is the standard choice for switching a 240V AC load on and off, since it interrupts both line conductors simultaneously with a single actuator while leaving the circuit routing straightforward. DPDT is needed when the application requires switching between two states or two output paths - motor direction reversal being the most common industrial example - rather than simple on/off isolation of both conductors. Using a single-pole switch on a 240V circuit leaves one conductor permanently connected regardless of switch position, which is an unsafe installation regardless of the switch's voltage rating.

What IP rating do I need for a rocker switch in an industrial panel?

The appropriate IP rating depends on what the switch face is exposed to, not the interior of the panel. A rocker switch in a sealed enclosure that never opens during operation has different exposure than one mounted on an operator station door subject to coolant splash or cleaning spray. IP54 provides protection against dust ingress and splash from any direction and covers most general industrial panel applications. IP65 adds full dust exclusion and protection against water jets, making it the appropriate minimum where washdown or direct coolant exposure is possible. Confirm the IP rating applies to the switch body as mounted, since many ratings assume the switch is installed in a panel cutout with the rear of the body inside the enclosure.